A1000 Drive
FAQs
Question | Posted Date | |
---|---|---|
Will there be a remote keypad option for the A1000? |
01/04/2011 | |
Where is the A1000 manufactured? |
01/04/2011 | |
Where does the A1000 fit into Yaskawa's family of drives, and what does it offer beyond the F7? |
01/03/2011 | |
When will single phase input capacities be available for A1000 and what kind of derating is expected? |
01/03/2011 | |
When using 2 option cards, I am receiving an OPE06 fault and am not seeing all the F1 parameters. I am using CN5-B for my encoder feedback card. |
10/09/2012 | |
What training is available for A1000? |
01/03/2011 | |
What tools are available to help customers convert from G5 (600V) and F7 to A1000? |
01/03/2011 | |
What is the warranty determination for new product? |
05/22/2014 | |
What is the scan rate of the A1000? |
01/04/2011 | |
What is RoHS? |
08/18/2015 | |
What is EN61800-5-1 and TUV? |
01/04/2011 | |
What is California's Proposition 65? |
06/01/2020 | |
What do I do if I am having problems connecting to the A1000 USB port? |
09/27/2011 | |
What documentation ships with the A1000? |
01/03/2011 | |
What control methods does the A1000 offer? |
01/04/2011 | |
What are the new capabilities of DriveWizard Industrial, and will it be backward compatible? |
01/14/2019 | |
What are the differences between the A1000 600V and A1000 240/480V models? |
01/04/2011 | |
What are the details regarding A1000 12 Pulse? |
05/30/2012 | |
What are the A1000's ratings? |
01/04/2011 | |
What A1000 enclosure types are available? |
01/03/2011 | |
On the A1000 series, if a unidirectional 3-wire control is desired, can the directional digital input (H1-0X = 0) be disabled? |
11/13/2013 | |
My drive has a CPF25 fault on it, my V1000 manual has no information on this alarm. What are some troubleshooting techniques to apply? |
10/29/2012 | |
Is the A1000 the same physical size as F7? |
01/04/2011 | |
Is the A1000 dual rated? |
01/04/2011 | |
In Normal Duty mode, is the default carrier frequency higher than 2kHz? |
01/04/2011 | |
If the drives carrier frequency is changed , is it necessary to re-autotune the drive? |
04/09/2012 | |
I am writing to the speed reference register using MODBUS TCP/IP for my 1000 series drive, yet U1-01 does not read properly. I can write to other registers with no problem. What are my possible issues? |
08/13/2013 | |
I am using the MOP function on the 7 series drives and on my deceleration; the drive is following the speed pot instead of the deceleration time. Why is that? |
02/28/2013 | |
How to change motor direction when rotating backwards? |
10/30/2012 | |
How do I save and recall parameter settings for User Initialization? |
02/28/2013 | |
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.