Controller Firmware
Additional Information
Firmware is valid for these applicable products:
Notes:
- Firmware refers to the operational code that resides on the physical hardware.
- Firmware Library refers to the function block interface, or FWL file, that contains the PLCopen and Yaskawa function blocks used in a MotionWorks IEC application program. The firmware libraries should not be confused with a PLCopen Toolbox, which is an application level set of programming tools also available.
Node: lr2